Waveform

This is a source sequence parameter which specifies the waveform to be generated.

The alternatives which can be selected from the dropdown list are:

Waveform File Types

The file types which can be selected for this parameter are: *.bin, *.wfm, *.waveform, and *.seq.

Note: A waveform sequence file (with the filename extension ".seq") is a composite waveform file; it is unrelated to a an EXT sequence file (which has the same extension, and is used when saving a sequence from Sequence Studio).

Waveform Must Be In Arb Memory

If the Waveform parameter is set to the name of a file, that file must be loaded from the D:\NVARB directory to the ARB memory of the source in the EXT test set before the sequence is run. If the referenced waveform file is not in ARB memory, an error window appears, as follows:

This situation can be remedied either through the front panel interface of the EXT test set (in the menu Source, Modulation Setup, ARB, Select Waveform) or by sending SCPI commands from the Interactive I/O tab of Sequence Studio.

To load a given file to ARB memory by means of a command, the format is:

:SOURce:RADio:ARB:LOAD "<file path>"

For example:

:SOUR:RAD:ARB:LOAD "D:\NVARB\EDGE_BURST.WFM"

To see the list of waveforms that are currently loaded into ARB memory, send the query:

:SOUR:RAD:ARB:CAT?